Modifier and Type | Method and Description |
---|---|
TaggedObject |
find(String journalIdentifier)
Finds the
TaggedObject with the given identifier as recorded in a journal. |
TaggedObject |
findObject(String journalIdentifier)
Finds the
ModelStaticIPA or ModelDynamicIPA with the given identifier as recorded in a journal. |
TaggedObject findObject(String journalIdentifier) throws NXException, RemoteException
ModelStaticIPA
or ModelDynamicIPA
with the given identifier as recorded in a journal.
An object may not return the same value as its JournalIdentifier in different versions of
the software. However newer versions of the software should find the same object when
FindObject is passed older versions of its journal identifier. In general, this method
should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
journalIdentifier
- Name of the IPA to be foundNXException
RemoteException
TaggedObject find(String journalIdentifier) throws NXException, RemoteException
TaggedObject
with the given identifier as recorded in a journal.
An object may not return the same value as its JournalIdentifier in different versions of
the software. However newer versions of the software should find the same object when
Find is passed older versions of its journal identifier. In general, this method
should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
journalIdentifier
- Identifier of the TaggedObject
to be foundNXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.