Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.menubar |
Provides classes and interfaces for the Menu Bar.
|
Class and Description |
---|
MenuBarManager
Interface for the MenuBarManager object
To obtain an instance of this class, refer to UI Created in NX6.0.0 |
Class and Description |
---|
ContextMenu
Represents a Context Menu .
|
ContextMenuEntry
Represents an entry on a context menu.
|
ContextMenuEntry.Type
Specifies the type of the menu entry.
|
ContextMenuProperties
Provides information about the MenuBar.ContextMenu object being customized.
|
MenuBarManager.ActionCallback
Prototype for the action callbacks
|
MenuBarManager.CallbackStatus
Return values for action callbacks
|
MenuBarManager.ConfigureContextMenu
Prototype for the callback used to configure a context menu.
|
MenuBarManager.EnterMenuApplication
Prototype for callback called whenever the application is entered
|
MenuBarManager.ExitMenuApplication
Prototype for callback called whenever the application is exited
|
MenuBarManager.InitializeMenuApplication
Prototype for application initialization callback
|
MenuButton
Implements the Object for Menu Buttons .
|
MenuButton.SensitivityStatus
Sensitivity Status
|
MenuButton.Toggle
Toggle Status
|
MenuButton.Type
Available button types
|
MenuButtonEvent
Implements the Event Object for Menu Buttons .
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.