Package | Description |
---|---|
nxopen.mechatronics |
Provides classes and interfaces for Mechatronics.
|
Modifier and Type | Field and Description |
---|---|
SymbolTableBuilder.IOType |
SymbolTableBuilder.Symbol.eIOType
IO type
|
static SymbolTableBuilder.IOType |
SymbolTableBuilder.IOType.INOUT
Input/Output
|
static SymbolTableBuilder.IOType |
SymbolTableBuilder.IOType.INPUT
Input
|
static SymbolTableBuilder.IOType |
SymbolTableBuilder.IOType.OUTPUT
Output
|
Modifier and Type | Method and Description |
---|---|
static SymbolTableBuilder.IOType |
SymbolTableBuilder.IOType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SymbolTableBuilder.IOType |
SymbolTableBuilder.IOType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SymbolTableBuilder.IOType[] |
SymbolTableBuilder.IOType.values()
Returns an array that contains the values for this enum.
|
Constructor and Description |
---|
Symbol(String nameInitial,
SymbolTableBuilder.IOType eIOTypeInitial,
SymbolTableBuilder.DataType eDataTypeInitial,
String addressInitial,
String commentInitial)
Constructor for the Symbol object.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.