Package | Description |
---|---|
nxopen.mechatronics |
Provides classes and interfaces for Mechatronics.
|
Modifier and Type | Field and Description |
---|---|
static SpeedPositionControlDirectiontype |
SpeedPositionControlDirectiontype.PARALLEL
parallel
|
static SpeedPositionControlDirectiontype |
SpeedPositionControlDirectiontype.PERPENDICULAR
perpendicular
|
Modifier and Type | Method and Description |
---|---|
SpeedPositionControlDirectiontype |
SpeedControlBuilder.directionType()
Returns the direction type, which works only when the speed control is used to
drive
TransportSurface
License requirements: None. |
SpeedPositionControlDirectiontype |
PositionControlBuilder.directionType()
Returns the direction type, which works only when the position control is used to
drive
TransportSurface
License requirements: nx_mcd_core ("MECHATRONICS CONCEPT DESIGNER") Created in NX10.0.0 |
static SpeedPositionControlDirectiontype |
SpeedPositionControlDirectiontype.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SpeedPositionControlDirectiontype |
SpeedPositionControlDirectiontype.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SpeedPositionControlDirectiontype[] |
SpeedPositionControlDirectiontype.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SpeedControlBuilder.setDirectionType(SpeedPositionControlDirectiontype directionType)
License requirements: nx_mcd_core ("MECHATRONICS CONCEPT DESIGNER") . |
void |
PositionControlBuilder.setDirectionType(SpeedPositionControlDirectiontype directionType)
License requirements: nx_mcd_core ("MECHATRONICS CONCEPT DESIGNER") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.