Package | Description |
---|---|
nxopen.mechatronics |
Provides classes and interfaces for Mechatronics.
|
Modifier and Type | Method and Description |
---|---|
SignalMappingConnectionBuilder |
SignalMappingConnectionCollection.createConnectionBuilder(SignalMappingConnection connection)
Creates a
SignalMappingConnectionBuilder
License requirements: nx_mcd_core ("MECHATRONICS CONCEPT DESIGNER") Created in NX12.0.0 |
SignalMappingConnectionBuilder |
SignalMappingConnectionBuilderList.findItem(int index)
Returns the object at the input index.
|
SignalMappingConnectionBuilder[] |
SignalMappingConnectionBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
SignalMappingConnectionBuilderList.append(SignalMappingConnectionBuilder object)
Appends an object to the list
License requirements: None. |
void |
SignalMappingConnectionBuilderList.append(SignalMappingConnectionBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
SignalMappingConnectionBuilderList.erase(SignalMappingConnectionBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
SignalMappingConnectionBuilderList.erase(SignalMappingConnectionBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
SignalMappingConnectionBuilderList.findIndex(SignalMappingConnectionBuilder obj)
Finds the index where the input object appears.
|
void |
SignalMappingConnectionBuilderList.insert(int location,
SignalMappingConnectionBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
SignalMappingConnectionBuilderList.setContents(SignalMappingConnectionBuilder[] objects)
Sets the contents of the entire list.
|
void |
SignalMappingConnectionBuilderList.swap(SignalMappingConnectionBuilder object1,
SignalMappingConnectionBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.