Package | Description |
---|---|
nxopen.mechatronics |
Provides classes and interfaces for Mechatronics.
|
Modifier and Type | Method and Description |
---|---|
SignalConnectionBuilder |
SignalConnectionCollection.createSignalConnectionBuilder(SignalConnection connection)
Creates a
SignalConnectionBuilder
License requirements: nx_mcd_core ("MECHATRONICS CONCEPT DESIGNER") Created in NX8.5.0 |
SignalConnectionBuilder |
SignalConnectionBuilderList.findItem(int index)
Returns the object at the input index.
|
SignalConnectionBuilder[] |
SignalConnectionBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
SignalConnectionBuilderList.append(SignalConnectionBuilder object)
Appends an object to the list
License requirements: None. |
void |
SignalConnectionBuilderList.append(SignalConnectionBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
SignalConnectionBuilderList.erase(SignalConnectionBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
SignalConnectionBuilderList.erase(SignalConnectionBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
SignalConnectionBuilderList.findIndex(SignalConnectionBuilder obj)
Finds the index where the input object appears.
|
void |
SignalConnectionBuilderList.insert(int location,
SignalConnectionBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
SignalConnectionBuilderList.setContents(SignalConnectionBuilder[] objects)
Sets the contents of the entire list.
|
void |
SignalConnectionBuilderList.swap(SignalConnectionBuilder object1,
SignalConnectionBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.