Package | Description |
---|---|
nxopen.mechatronics |
Provides classes and interfaces for Mechatronics.
|
Modifier and Type | Method and Description |
---|---|
SHMSignalConnectionBuilder |
SHMSignalConnectionCollection.createSHMSignalConnectionBuilder(SHMSignalConnection connection)
Creates a
SHMSignalConnectionBuilder
License requirements: nx_mcd_core ("MECHATRONICS CONCEPT DESIGNER") Created in NX9.0.0 |
SHMSignalConnectionBuilder |
SHMSignalConnectionBuilderList.findItem(int index)
Returns the object at the input index.
|
SHMSignalConnectionBuilder[] |
SHMSignalConnectionBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
SHMSignalConnectionBuilderList.append(SHMSignalConnectionBuilder object)
Appends an object to the list
License requirements: None. |
void |
SHMSignalConnectionBuilderList.append(SHMSignalConnectionBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
SHMSignalConnectionBuilderList.erase(SHMSignalConnectionBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
SHMSignalConnectionBuilderList.erase(SHMSignalConnectionBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
SHMSignalConnectionBuilderList.findIndex(SHMSignalConnectionBuilder obj)
Finds the index where the input object appears.
|
void |
SHMSignalConnectionBuilderList.insert(int location,
SHMSignalConnectionBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
SHMSignalConnectionBuilderList.setContents(SHMSignalConnectionBuilder[] objects)
Sets the contents of the entire list.
|
void |
SHMSignalConnectionBuilderList.swap(SHMSignalConnectionBuilder object1,
SHMSignalConnectionBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.