Package | Description |
---|---|
nxopen.mechatronics |
Provides classes and interfaces for Mechatronics.
|
Modifier and Type | Method and Description |
---|---|
RuntimeFormulaParameterBuilder |
RuntimeFormulaCollection.createRuntimeFormulaParameterBuilder(RuntimeFormulaParameter obj)
Creates a
RuntimeFormulaParameterBuilder
License requirements: nx_mcd_core ("MECHATRONICS CONCEPT DESIGNER") Created in NX8.5.0 |
RuntimeFormulaParameterBuilder |
RuntimeFormulaParameterBuilderList.findItem(int index)
Returns the object at the input index.
|
RuntimeFormulaParameterBuilder[] |
RuntimeFormulaParameterBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
RuntimeFormulaParameterBuilderList.append(RuntimeFormulaParameterBuilder object)
Appends an object to the list
License requirements: None. |
void |
RuntimeFormulaParameterBuilderList.append(RuntimeFormulaParameterBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
RuntimeFormulaParameterBuilderList.erase(RuntimeFormulaParameterBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
RuntimeFormulaParameterBuilderList.erase(RuntimeFormulaParameterBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
RuntimeFormulaParameterBuilderList.findIndex(RuntimeFormulaParameterBuilder obj)
Finds the index where the input object appears.
|
void |
RuntimeFormulaParameterBuilderList.insert(int location,
RuntimeFormulaParameterBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
RuntimeFormulaParameterBuilderList.setContents(RuntimeFormulaParameterBuilder[] objects)
Sets the contents of the entire list.
|
void |
RuntimeFormulaParameterBuilderList.swap(RuntimeFormulaParameterBuilder object1,
RuntimeFormulaParameterBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.