Package | Description |
---|---|
nxopen.mechatronics |
Provides classes and interfaces for Mechatronics.
|
Modifier and Type | Method and Description |
---|---|
PathConstraintFrameBuilder |
PathConstraintFrameBuilderList.findItem(int index)
Returns the object at the input index.
|
PathConstraintFrameBuilder[] |
PathConstraintFrameBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
PathConstraintFrameBuilder |
PathConstraintJointBuilder.newPathFrame()
Creates a
PathConstraintFrameBuilder object. |
Modifier and Type | Method and Description |
---|---|
void |
PathConstraintFrameBuilderList.append(PathConstraintFrameBuilder object)
Appends an object to the list
License requirements: None. |
void |
PathConstraintFrameBuilderList.append(PathConstraintFrameBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
PathConstraintFrameBuilderList.erase(PathConstraintFrameBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
PathConstraintFrameBuilderList.erase(PathConstraintFrameBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
PathConstraintFrameBuilderList.findIndex(PathConstraintFrameBuilder obj)
Finds the index where the input object appears.
|
void |
PathConstraintFrameBuilderList.insert(int location,
PathConstraintFrameBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
PathConstraintFrameBuilderList.setContents(PathConstraintFrameBuilder[] objects)
Sets the contents of the entire list.
|
void |
PathConstraintFrameBuilderList.swap(PathConstraintFrameBuilder object1,
PathConstraintFrameBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.