Package | Description |
---|---|
nxopen.mechatronics |
Provides classes and interfaces for Mechatronics.
|
Modifier and Type | Method and Description |
---|---|
GanttOperationParameterBuilder |
GanttCollection.createGanttOperationParameterBuilder()
Creates a
GanttOperationParameterBuilder
License requirements: nx_mcd_core ("MECHATRONICS CONCEPT DESIGNER") Created in NX7.5.1 |
GanttOperationParameterBuilder |
GanttOperationParameterBuilderList.findItem(int index)
Returns the object at the input index.
|
GanttOperationParameterBuilder[] |
GanttOperationParameterBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
GanttOperationBuilder.addParameterList(GanttOperationParameterBuilder[] parameters)
Sets the parameter data
License requirements: nx_mcd_core ("MECHATRONICS CONCEPT DESIGNER") . |
void |
GanttOperationParameterBuilderList.append(GanttOperationParameterBuilder object)
Appends an object to the list
License requirements: None. |
void |
GanttOperationParameterBuilderList.append(GanttOperationParameterBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
GanttOperationParameterBuilderList.erase(GanttOperationParameterBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
GanttOperationParameterBuilderList.erase(GanttOperationParameterBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
GanttOperationParameterBuilderList.findIndex(GanttOperationParameterBuilder obj)
Finds the index where the input object appears.
|
void |
GanttOperationParameterBuilderList.insert(int location,
GanttOperationParameterBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
GanttOperationParameterBuilderList.setContents(GanttOperationParameterBuilder[] objects)
Sets the contents of the entire list.
|
void |
GanttOperationParameterBuilderList.swap(GanttOperationParameterBuilder object1,
GanttOperationParameterBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.