Package | Description |
---|---|
nxopen.mechatronics |
Provides classes and interfaces for Mechatronics.
|
Modifier and Type | Method and Description |
---|---|
ExternalConnectionElementBuilder |
ExternalConnectionCollection.createExternalConnectionElementBuilder(ExternalConnectionElement element)
Creates a
ExternalConnectionElementBuilder
License requirements: nx_mcd_core ("MECHATRONICS CONCEPT DESIGNER") Created in NX8.0.1 |
ExternalConnectionElementBuilder |
ExternalConnectionElementBuilderList.findItem(int index)
Returns the object at the input index.
|
ExternalConnectionElementBuilder[] |
ExternalConnectionElementBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
ExternalConnectionElementBuilderList.append(ExternalConnectionElementBuilder object)
Appends an object to the list
License requirements: None. |
void |
ExternalConnectionElementBuilderList.append(ExternalConnectionElementBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
ExternalConnectionElementBuilderList.erase(ExternalConnectionElementBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
ExternalConnectionElementBuilderList.erase(ExternalConnectionElementBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
ExternalConnectionElementBuilderList.findIndex(ExternalConnectionElementBuilder obj)
Finds the index where the input object appears.
|
void |
ExternalConnectionElementBuilderList.insert(int location,
ExternalConnectionElementBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
ExternalConnectionElementBuilderList.setContents(ExternalConnectionElementBuilder[] objects)
Sets the contents of the entire list.
|
void |
ExternalConnectionElementBuilderList.swap(ExternalConnectionElementBuilder object1,
ExternalConnectionElementBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.