Package | Description |
---|---|
nxopen.mechanicalrouting |
Provides classes and interfaces for Mechanical Routing.
|
Modifier and Type | Method and Description |
---|---|
PathTransitionBuilder |
PathTransitionListManagerBuilder.createPathTransitionBuilder(Part part)
Creates a
PathTransitionBuilder object. |
PathTransitionBuilder |
PathTransitionBuilderList.findItem(int index)
Returns the object at the input index.
|
PathTransitionBuilder[] |
PathTransitionBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
PathTransitionBuilderList.append(PathTransitionBuilder object)
Appends an object to the list
License requirements: None. |
void |
PathTransitionBuilderList.append(PathTransitionBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
PathTransitionBuilderList.erase(PathTransitionBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
PathTransitionBuilderList.erase(PathTransitionBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
PathTransitionBuilderList.findIndex(PathTransitionBuilder obj)
Finds the index where the input object appears.
|
void |
PathTransitionBuilderList.insert(int location,
PathTransitionBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
PathTransitionBuilderList.setContents(PathTransitionBuilder[] objects)
Sets the contents of the entire list.
|
void |
PathTransitionBuilderList.swap(PathTransitionBuilder object1,
PathTransitionBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.