Package | Description |
---|---|
nxopen.mechanicalrouting |
Provides classes and interfaces for Mechanical Routing.
|
Modifier and Type | Field and Description |
---|---|
static PathTransitionBuilder.Type |
PathTransitionBuilder.Type.DIRECT |
static PathTransitionBuilder.Type |
PathTransitionBuilder.Type.HEAL |
static PathTransitionBuilder.Type |
PathTransitionBuilder.Type.INTERSECT |
Modifier and Type | Method and Description |
---|---|
PathTransitionBuilder.Type |
PathTransitionBuilder.transitionType()
Returns the type of transition the path takes to reach the transition end point.
|
static PathTransitionBuilder.Type |
PathTransitionBuilder.Type.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PathTransitionBuilder.Type |
PathTransitionBuilder.Type.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PathTransitionBuilder.Type[] |
PathTransitionBuilder.Type.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PathTransitionBuilder.setTransitionType(PathTransitionBuilder.Type transitionType)
License requirements: routing_base ("Routing Basic") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.