Package | Description |
---|---|
nxopen.mechanicalrouting |
Provides classes and interfaces for Mechanical Routing.
|
Modifier and Type | Field and Description |
---|---|
static PartPlacementBuilder.PlacementValidationStatus |
PartPlacementBuilder.PlacementValidationStatus.PART_NOT_CONNECTED_TO_ROUT
after placement connection should have been built with routing system but it was not
|
static PartPlacementBuilder.PlacementValidationStatus |
PartPlacementBuilder.PlacementValidationStatus.SUCCESS
part placement is successful as expected
|
Modifier and Type | Method and Description |
---|---|
PartPlacementBuilder.PlacementValidationStatus |
PartPlacementBuilder.commitThisPlacement()
Commits the current placement operation.
|
static PartPlacementBuilder.PlacementValidationStatus |
PartPlacementBuilder.PlacementValidationStatus.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PartPlacementBuilder.PlacementValidationStatus |
PartPlacementBuilder.PlacementValidationStatus.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PartPlacementBuilder.PlacementValidationStatus[] |
PartPlacementBuilder.PlacementValidationStatus.values()
Returns an array that contains the values for this enum.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.