Package | Description |
---|---|
nxopen.mechanicalrouting |
Provides classes and interfaces for Mechanical Routing.
|
Modifier and Type | Field and Description |
---|---|
static MovePathBuilder.DetachTypes |
MovePathBuilder.DetachTypes.ALLOW_DETACH_ON_CONFLICT |
static MovePathBuilder.DetachTypes |
MovePathBuilder.DetachTypes.ALWAYS_MAINTAIN_CONNECTIONS |
static MovePathBuilder.DetachTypes |
MovePathBuilder.DetachTypes.DETACH_SELECTED_OBJECTS |
Modifier and Type | Method and Description |
---|---|
MovePathBuilder.DetachTypes |
MovePathBuilder.detachType()
Returns the detach type setting.
|
static MovePathBuilder.DetachTypes |
MovePathBuilder.DetachTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MovePathBuilder.DetachTypes |
MovePathBuilder.DetachTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MovePathBuilder.DetachTypes[] |
MovePathBuilder.DetachTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MovePathBuilder.setDetachType(MovePathBuilder.DetachTypes detachType)
License requirements: routing_base ("Routing Basic") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.