Package | Description |
---|---|
nxopen.mechanicalrouting |
Provides classes and interfaces for Mechanical Routing.
|
Modifier and Type | Field and Description |
---|---|
static InsulationBuilder.WrapType |
InsulationBuilder.WrapType.NO_WARP
No wrapping
|
static InsulationBuilder.WrapType |
InsulationBuilder.WrapType.OVERLAP_SPIRAL
Overlap Spiral
|
static InsulationBuilder.WrapType |
InsulationBuilder.WrapType.STRIPED_SPIRAL
Striped Spiral
|
Modifier and Type | Method and Description |
---|---|
InsulationBuilder.WrapType |
InsulationBuilder.suggestWrapMethodBasedOnStockSettings()
Returns the suggestion for
InsulationBuilder.WrapType based on
PathStockPreferenceBuilder
License requirements: routing_base ("Routing Basic") Created in NX11.0.1 |
static InsulationBuilder.WrapType |
InsulationBuilder.WrapType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InsulationBuilder.WrapType |
InsulationBuilder.WrapType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InsulationBuilder.WrapType[] |
InsulationBuilder.WrapType.values()
Returns an array that contains the values for this enum.
|
InsulationBuilder.WrapType |
InsulationBuilder.wrapMethod()
Returns the
InsulationBuilder.WrapType for Wrapped Insulation. |
Modifier and Type | Method and Description |
---|---|
void |
InsulationBuilder.setWrapMethod(InsulationBuilder.WrapType wrapMethod)
License requirements: routing_base ("Routing Basic") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.