Package | Description |
---|---|
nxopen.mechanicalrouting |
Provides classes and interfaces for Mechanical Routing.
|
Modifier and Type | Field and Description |
---|---|
static EditPointBuilder.Editsegmenttype |
EditPointBuilder.Editsegmenttype.ANGLE
Edit angle type in Edit Segment Motion
|
static EditPointBuilder.Editsegmenttype |
EditPointBuilder.Editsegmenttype.LENGTH
Edit length type in Edit Segment Motion
|
static EditPointBuilder.Editsegmenttype |
EditPointBuilder.Editsegmenttype.NONE
Move Point Motion
|
Modifier and Type | Method and Description |
---|---|
EditPointBuilder.Editsegmenttype |
EditPointBuilder.activeEditSegmentType()
Returns the edit segment type setting
Allows you to specify the type of edit in edit segment motion.
|
static EditPointBuilder.Editsegmenttype |
EditPointBuilder.Editsegmenttype.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EditPointBuilder.Editsegmenttype |
EditPointBuilder.Editsegmenttype.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EditPointBuilder.Editsegmenttype[] |
EditPointBuilder.Editsegmenttype.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EditPointBuilder.setActiveEditSegmentType(EditPointBuilder.Editsegmenttype editSegmentType)
License requirements: routing_base ("Routing Basic") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.