Package | Description |
---|---|
nxopen.mechanicalrouting |
Provides classes and interfaces for Mechanical Routing.
|
Modifier and Type | Field and Description |
---|---|
static CornerBuilder.Type |
CornerBuilder.Type.BEND
allows corner creation with the specified bend type
|
static CornerBuilder.Type |
CornerBuilder.Type.MITER
allows miter corner creation
|
static CornerBuilder.Type |
CornerBuilder.Type.NONE
None, no corner created
|
Modifier and Type | Method and Description |
---|---|
CornerBuilder.Type |
CornerBuilder.cornerType()
Returns the corner types
License requirements: routing_base ("Routing Basic") . |
static CornerBuilder.Type |
CornerBuilder.Type.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CornerBuilder.Type |
CornerBuilder.Type.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CornerBuilder.Type[] |
CornerBuilder.Type.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CornerBuilder.setCornerType(CornerBuilder.Type cornerType)
License requirements: routing_base ("Routing Basic") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.