Package | Description |
---|---|
nxopen.mechanicalrouting |
Provides classes and interfaces for Mechanical Routing.
|
Modifier and Type | Field and Description |
---|---|
static BendCornerTypeBuilder.BendMethod |
BendCornerTypeBuilder.BendMethod.BEND_RADIUS_TABLE
Bend table method creates bend from specified bend table
|
static BendCornerTypeBuilder.BendMethod |
BendCornerTypeBuilder.BendMethod.INNER_RADIUS
Inner Radius method allows corner creation with the specified inner radius value
|
static BendCornerTypeBuilder.BendMethod |
BendCornerTypeBuilder.BendMethod.RADIUS
Radius method allows corner creation with the specified radius value
|
static BendCornerTypeBuilder.BendMethod |
BendCornerTypeBuilder.BendMethod.RATIO_TO_DIAMETER
Ratio to diameter method
|
Modifier and Type | Method and Description |
---|---|
BendCornerTypeBuilder.BendMethod |
BendCornerTypeBuilder.method()
Returns the bend corner methods
License requirements: routing_base ("Routing Basic") . |
static BendCornerTypeBuilder.BendMethod |
BendCornerTypeBuilder.BendMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BendCornerTypeBuilder.BendMethod |
BendCornerTypeBuilder.BendMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BendCornerTypeBuilder.BendMethod[] |
BendCornerTypeBuilder.BendMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BendCornerTypeBuilder.setMethod(BendCornerTypeBuilder.BendMethod routeCornerBendMethods)
License requirements: routing_base ("Routing Basic") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.