Package | Description |
---|---|
nxopen.markup |
Provides classes and interfaces for Markup.
|
Modifier and Type | Interface and Description |
---|---|
interface |
Circle
Represents a
Circle
To create a new instance of this class, use MarkupFileObjectCollection.createCircle(nxopen.Point2d, double) Created in NX10.0.0 NX_REMOVE_FROM_JAVA_API |
interface |
Ellipse
Represents a
Ellipse
To create a new instance of this class, use MarkupFileObjectCollection.createEllipse(nxopen.Point2d, double, double) Created in NX10.0.0 NX_REMOVE_FROM_JAVA_API |
interface |
Freehand
Represents a
Freehand
To create a new instance of this class, use MarkupFileObjectCollection.createFreehand(nxopen.Point2d[]) Created in NX10.0.0 NX_REMOVE_FROM_JAVA_API |
interface |
Icon
Represents a
Icon
To create a new instance of this class, use MarkupFileObjectCollection.createIcon(nxopen.Point2d, java.lang.String, nxopen.markup.Icon.Size) Created in NX10.0.0 NX_REMOVE_FROM_JAVA_API |
interface |
Polyline
Represents a
Polyline
To create a new instance of this class, use MarkupFileObjectCollection.createPolyline(nxopen.Point2d[]) Created in NX10.0.0 NX_REMOVE_FROM_JAVA_API |
interface |
Rectangle
Represents a
Rectangle
To create a new instance of this class, use MarkupFileObjectCollection.createRectangle(nxopen.Point2d, double, double) Created in NX10.0.0 NX_REMOVE_FROM_JAVA_API |
interface |
Text
Represents a
Text
To create a new instance of this class, use MarkupFileObjectCollection.createText(nxopen.Point2d, java.lang.String) Created in NX10.0.0 NX_REMOVE_FROM_JAVA_API |
Modifier and Type | Method and Description |
---|---|
MarkupObject |
MarkupObjectCollection.findObject(String id)
Finds the
MarkupObject with the given id. |
MarkupObject |
MarkupFileObjectCollection.findObject(String id)
Finds the
MarkupObject with the given id in current file. |
Modifier and Type | Method and Description |
---|---|
EditObjectDisplayBuilder |
MarkupFileCollection.createEditObjectDisplayBuilder(MarkupObject[] objects)
Creates a
EditObjectDisplayBuilder
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.