Package | Description |
---|---|
nxopen.markup |
Provides classes and interfaces for Markup.
|
Modifier and Type | Field and Description |
---|---|
static Icon.Size |
Icon.Size.EXTRA_SMALL
Extra small size
|
static Icon.Size |
Icon.Size.LARGE
Large size
|
static Icon.Size |
Icon.Size.MEDIUM
Medium size
|
static Icon.Size |
Icon.Size.SMALL
Small size
|
Modifier and Type | Method and Description |
---|---|
Icon.Size |
Icon.iconSize()
Returns the icon size.
|
static Icon.Size |
Icon.Size.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Icon.Size |
Icon.Size.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Icon.Size[] |
Icon.Size.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
Icon |
MarkupFileObjectCollection.createIcon(Point2d position,
String iconName,
Icon.Size size)
Creates a
Icon
License requirements: None. |
void |
Icon.setIconSize(Icon.Size size)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.