Package | Description |
---|---|
nxopen.linedesigner |
Provides classes and interfaces for Line Designer.
|
Modifier and Type | Field and Description |
---|---|
static RailingFeatureBuilder.PostOffsetType |
RailingFeatureBuilder.PostOffsetType.POST_LEFT_OF_CURVE |
static RailingFeatureBuilder.PostOffsetType |
RailingFeatureBuilder.PostOffsetType.POST_ON_CURVE |
static RailingFeatureBuilder.PostOffsetType |
RailingFeatureBuilder.PostOffsetType.POST_RIGHT_OF_CURVE |
Modifier and Type | Method and Description |
---|---|
RailingFeatureBuilder.PostOffsetType |
RailingFeatureBuilder.postOffset()
Returns the post offset of railing feature
License requirements: ld_line_designer ("FULL LINE DESIGNER") . |
static RailingFeatureBuilder.PostOffsetType |
RailingFeatureBuilder.PostOffsetType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RailingFeatureBuilder.PostOffsetType |
RailingFeatureBuilder.PostOffsetType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RailingFeatureBuilder.PostOffsetType[] |
RailingFeatureBuilder.PostOffsetType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
RailingFeatureBuilder.setPostOffset(RailingFeatureBuilder.PostOffsetType postOffset)
License requirements: ld_line_designer ("FULL LINE DESIGNER") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.