Package | Description |
---|---|
nxopen.linedesigner |
Provides classes and interfaces for Line Designer.
|
Modifier and Type | Field and Description |
---|---|
static PlatformEquipmentBuilder.SideFromCenterlineTypeAPI |
PlatformEquipmentBuilder.SideFromCenterlineTypeAPI.LEFT_BOTTOM_SIDE |
static PlatformEquipmentBuilder.SideFromCenterlineTypeAPI |
PlatformEquipmentBuilder.SideFromCenterlineTypeAPI.RIGHT_TOP_SIDE |
Modifier and Type | Method and Description |
---|---|
PlatformEquipmentBuilder.SideFromCenterlineTypeAPI |
PlatformEquipmentBuilder.sideFromCenterlineEnum()
Returns the side from center line
License requirements: ld_line_designer ("FULL LINE DESIGNER") . |
static PlatformEquipmentBuilder.SideFromCenterlineTypeAPI |
PlatformEquipmentBuilder.SideFromCenterlineTypeAPI.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PlatformEquipmentBuilder.SideFromCenterlineTypeAPI |
PlatformEquipmentBuilder.SideFromCenterlineTypeAPI.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PlatformEquipmentBuilder.SideFromCenterlineTypeAPI[] |
PlatformEquipmentBuilder.SideFromCenterlineTypeAPI.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PlatformEquipmentBuilder.setSideFromCenterlineEnum(PlatformEquipmentBuilder.SideFromCenterlineTypeAPI sideFromCenterlineEnum)
License requirements: ld_line_designer ("FULL LINE DESIGNER") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.