Package | Description |
---|---|
nxopen.linedesigner |
Provides classes and interfaces for Line Designer.
|
Modifier and Type | Field and Description |
---|---|
static PlatformEquipmentBuilder.DeckingMaterialTypeAPI |
PlatformEquipmentBuilder.DeckingMaterialTypeAPI.CHECKER_PLATE |
static PlatformEquipmentBuilder.DeckingMaterialTypeAPI |
PlatformEquipmentBuilder.DeckingMaterialTypeAPI.METAL_GRATE |
Modifier and Type | Method and Description |
---|---|
PlatformEquipmentBuilder.DeckingMaterialTypeAPI |
PlatformEquipmentBuilder.deckingMaterial()
Returns the decking material
License requirements: ld_line_designer ("FULL LINE DESIGNER") . |
static PlatformEquipmentBuilder.DeckingMaterialTypeAPI |
PlatformEquipmentBuilder.DeckingMaterialTypeAPI.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PlatformEquipmentBuilder.DeckingMaterialTypeAPI |
PlatformEquipmentBuilder.DeckingMaterialTypeAPI.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PlatformEquipmentBuilder.DeckingMaterialTypeAPI[] |
PlatformEquipmentBuilder.DeckingMaterialTypeAPI.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PlatformEquipmentBuilder.setDeckingMaterial(PlatformEquipmentBuilder.DeckingMaterialTypeAPI deckingMaterial)
License requirements: ld_line_designer ("FULL LINE DESIGNER") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.