Package | Description |
---|---|
nxopen.linedesigner |
Provides classes and interfaces for Line Designer.
|
Modifier and Type | Field and Description |
---|---|
static PlatformEquipmentBuilder.DeckSupportTypeAPI |
PlatformEquipmentBuilder.DeckSupportTypeAPI.AUTOMATIC_SUPPORTIN_GRID_PATTERN |
static PlatformEquipmentBuilder.DeckSupportTypeAPI |
PlatformEquipmentBuilder.DeckSupportTypeAPI.CORNERS_SUPPORTS_ONLY |
static PlatformEquipmentBuilder.DeckSupportTypeAPI |
PlatformEquipmentBuilder.DeckSupportTypeAPI.MANUAL_SUPPORTS |
static PlatformEquipmentBuilder.DeckSupportTypeAPI |
PlatformEquipmentBuilder.DeckSupportTypeAPI.NO_SUPPORTS |
Modifier and Type | Method and Description |
---|---|
PlatformEquipmentBuilder.DeckSupportTypeAPI |
PlatformEquipmentBuilder.deckSupportEnum()
Returns the deck support type for platform
License requirements: ld_line_designer ("FULL LINE DESIGNER") . |
static PlatformEquipmentBuilder.DeckSupportTypeAPI |
PlatformEquipmentBuilder.DeckSupportTypeAPI.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PlatformEquipmentBuilder.DeckSupportTypeAPI |
PlatformEquipmentBuilder.DeckSupportTypeAPI.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PlatformEquipmentBuilder.DeckSupportTypeAPI[] |
PlatformEquipmentBuilder.DeckSupportTypeAPI.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PlatformEquipmentBuilder.setDeckSupportEnum(PlatformEquipmentBuilder.DeckSupportTypeAPI deckSupportEnum)
License requirements: ld_line_designer ("FULL LINE DESIGNER") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.