Package | Description |
---|---|
nxopen.linedesigner |
Provides classes and interfaces for Line Designer.
|
Modifier and Type | Field and Description |
---|---|
static InsertSheetBuilder.APIUnits |
InsertSheetBuilder.APIUnits.INCHES
Represents the Inches type
|
static InsertSheetBuilder.APIUnits |
InsertSheetBuilder.APIUnits.MILLIMETERS
Represents the Millimeters type
|
Modifier and Type | Method and Description |
---|---|
InsertSheetBuilder.APIUnits |
InsertSheetBuilder.unitsEnum()
Returns the units enum
License requirements: ld_line_designer ("FULL LINE DESIGNER") . |
static InsertSheetBuilder.APIUnits |
InsertSheetBuilder.APIUnits.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InsertSheetBuilder.APIUnits |
InsertSheetBuilder.APIUnits.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InsertSheetBuilder.APIUnits[] |
InsertSheetBuilder.APIUnits.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
InsertSheetBuilder.setUnitsEnum(InsertSheetBuilder.APIUnits unitsEnum)
License requirements: ld_line_designer ("FULL LINE DESIGNER") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.