Package | Description |
---|---|
nxopen.linedesigner |
Provides classes and interfaces for Line Designer.
|
Modifier and Type | Field and Description |
---|---|
static GateFeatureBuilder.GateOpeningStyle |
GateFeatureBuilder.GateOpeningStyle.LEFT |
static GateFeatureBuilder.GateOpeningStyle |
GateFeatureBuilder.GateOpeningStyle.MIDDLE |
static GateFeatureBuilder.GateOpeningStyle |
GateFeatureBuilder.GateOpeningStyle.RIGHT |
Modifier and Type | Method and Description |
---|---|
GateFeatureBuilder.GateOpeningStyle |
GateFeatureBuilder.openingStyleEnum()
Returns the opening style of gate
License requirements: ld_line_designer ("FULL LINE DESIGNER") . |
static GateFeatureBuilder.GateOpeningStyle |
GateFeatureBuilder.GateOpeningStyle.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GateFeatureBuilder.GateOpeningStyle |
GateFeatureBuilder.GateOpeningStyle.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GateFeatureBuilder.GateOpeningStyle[] |
GateFeatureBuilder.GateOpeningStyle.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GateFeatureBuilder.setOpeningStyleEnum(GateFeatureBuilder.GateOpeningStyle openingStyleEnum)
License requirements: ld_line_designer ("FULL LINE DESIGNER") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.