Package | Description |
---|---|
nxopen.linedesigner |
Provides classes and interfaces for Line Designer.
|
Modifier and Type | Field and Description |
---|---|
static ExportToDWGBuilder.SaveAsTypeAPI |
ExportToDWGBuilder.SaveAsTypeAPI.T2D
Represents the 2D type
|
static ExportToDWGBuilder.SaveAsTypeAPI |
ExportToDWGBuilder.SaveAsTypeAPI.T3D
Represents the 3D type
|
Modifier and Type | Method and Description |
---|---|
ExportToDWGBuilder.SaveAsTypeAPI |
ExportToDWGBuilder.saveAs()
Returns an API to get save as type
License requirements: ld_line_designer ("FULL LINE DESIGNER") . |
static ExportToDWGBuilder.SaveAsTypeAPI |
ExportToDWGBuilder.SaveAsTypeAPI.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ExportToDWGBuilder.SaveAsTypeAPI |
ExportToDWGBuilder.SaveAsTypeAPI.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ExportToDWGBuilder.SaveAsTypeAPI[] |
ExportToDWGBuilder.SaveAsTypeAPI.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ExportToDWGBuilder.setSaveAs(ExportToDWGBuilder.SaveAsTypeAPI saveAs)
License requirements: ld_line_designer ("FULL LINE DESIGNER") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.