Package | Description |
---|---|
nxopen.linedesigner |
Provides classes and interfaces for Line Designer.
|
Modifier and Type | Field and Description |
---|---|
static ColumnGridEquipmentBuilder.ColumnBaseType |
ColumnGridEquipmentBuilder.ColumnBaseType.CIRCLE |
static ColumnGridEquipmentBuilder.ColumnBaseType |
ColumnGridEquipmentBuilder.ColumnBaseType.CONE |
static ColumnGridEquipmentBuilder.ColumnBaseType |
ColumnGridEquipmentBuilder.ColumnBaseType.NONE |
static ColumnGridEquipmentBuilder.ColumnBaseType |
ColumnGridEquipmentBuilder.ColumnBaseType.RECTANGLE |
static ColumnGridEquipmentBuilder.ColumnBaseType |
ColumnGridEquipmentBuilder.ColumnBaseType.USER_DEFINE |
Modifier and Type | Method and Description |
---|---|
ColumnGridEquipmentBuilder.ColumnBaseType |
ColumnGridEquipmentBuilder.columnBaseTypeEnum()
Returns the column base type of column grid
License requirements: ld_line_designer ("FULL LINE DESIGNER") . |
static ColumnGridEquipmentBuilder.ColumnBaseType |
ColumnGridEquipmentBuilder.ColumnBaseType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ColumnGridEquipmentBuilder.ColumnBaseType |
ColumnGridEquipmentBuilder.ColumnBaseType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ColumnGridEquipmentBuilder.ColumnBaseType[] |
ColumnGridEquipmentBuilder.ColumnBaseType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ColumnGridEquipmentBuilder.setColumnBaseTypeEnum(ColumnGridEquipmentBuilder.ColumnBaseType columnBaseTypeEnum)
Sets the column base type of column grid
License requirements: ld_line_designer ("FULL LINE DESIGNER") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.