Package | Description |
---|---|
nxopen.linedesigner |
Provides classes and interfaces for Line Designer.
|
Modifier and Type | Field and Description |
---|---|
static ColumnFeatureBuilder.ColumnBaseType |
ColumnFeatureBuilder.ColumnBaseType.CIRCLE |
static ColumnFeatureBuilder.ColumnBaseType |
ColumnFeatureBuilder.ColumnBaseType.CONE |
static ColumnFeatureBuilder.ColumnBaseType |
ColumnFeatureBuilder.ColumnBaseType.NONE |
static ColumnFeatureBuilder.ColumnBaseType |
ColumnFeatureBuilder.ColumnBaseType.RECTANGLE |
static ColumnFeatureBuilder.ColumnBaseType |
ColumnFeatureBuilder.ColumnBaseType.USER_DEFINED |
Modifier and Type | Method and Description |
---|---|
ColumnFeatureBuilder.ColumnBaseType |
ColumnFeatureBuilder.baseStyleEnum()
Returns the base cross section type of column feature
License requirements: ld_line_designer ("FULL LINE DESIGNER") . |
static ColumnFeatureBuilder.ColumnBaseType |
ColumnFeatureBuilder.ColumnBaseType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ColumnFeatureBuilder.ColumnBaseType |
ColumnFeatureBuilder.ColumnBaseType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ColumnFeatureBuilder.ColumnBaseType[] |
ColumnFeatureBuilder.ColumnBaseType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ColumnFeatureBuilder.setBaseStyleEnum(ColumnFeatureBuilder.ColumnBaseType baseStyleEnum)
Sets the base cross section type of column feature
License requirements: ld_line_designer ("FULL LINE DESIGNER") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.