Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static Type |
Type.NO_OFFSET
No offset
|
static Type |
Type.NONSYMMETRIC_OFFSET
Offset with two different distances
|
static Type |
Type.SINGLE_OFFSET
Offset with single distance in one direction
|
static Type |
Type.SYMMETRIC_OFFSET
Offset with same distance in both directions
|
Modifier and Type | Method and Description |
---|---|
Type |
FeatureOffset.option()
Returns the Offset option
License requirements: None. |
static Type |
Type.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Type |
Type.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Type[] |
Type.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FeatureOffset.setOption(Type offsetType)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.