Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Method and Description |
---|---|
TwoExpressionsSectionSet |
Part.createEmptyTwoExpressionsSectionSet()
Creates an empty TwoExpressionSectionSet item that contains
a
Section section
and two corresponding expressions
License requirements: None. |
TwoExpressionsSectionSet |
Part.createTwoExpressionsSectionSet(Section section,
String value,
String valueTwo,
String unitsType,
int index)
Creates an TwoExpressionSectionSet item that contains
a
Section section
and two corresponding expressions
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
TwoExpressionsSectionSet |
TwoExpressionsSectionSetList.findItem(int index)
Returns the object at the input index.
|
TwoExpressionsSectionSet[] |
TwoExpressionsSectionSetList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
TwoExpressionsSectionSetList.append(TwoExpressionsSectionSet object)
Appends an object to the list
License requirements: None. |
void |
TwoExpressionsSectionSetList.append(TwoExpressionsSectionSet[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
TwoExpressionsSectionSetList.erase(TwoExpressionsSectionSet obj)
Erases the object from the list, but does not delete the object.
|
void |
TwoExpressionsSectionSetList.erase(TwoExpressionsSectionSet obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
TwoExpressionsSectionSetList.findIndex(TwoExpressionsSectionSet obj)
Finds the index where the input object appears.
|
void |
TwoExpressionsSectionSetList.insert(int location,
TwoExpressionsSectionSet object)
Inserts an object at the specified location
License requirements: None. |
void |
TwoExpressionsSectionSetList.setContents(TwoExpressionsSectionSet[] objects)
Sets the contents of the entire list.
|
void |
TwoExpressionsSectionSetList.swap(TwoExpressionsSectionSet object1,
TwoExpressionsSectionSet object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.