Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Method and Description |
---|---|
TwoExpressionsCollectorSet |
Part.createEmptyTwoExpressionsCollectorSet()
Creates an empty TwoExpressionCollectorSet item that contains
a
ScCollector collection
and two corresponding expressions
License requirements: None. |
TwoExpressionsCollectorSet |
Part.createTwoExpressionsCollectorSet(ScCollector collector,
String value,
String valueTwo,
String unitsType,
int index)
Creates an TwoExpressionCollectorSet item that contains
a
ScCollector collection
and two corresponding expressions
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
TwoExpressionsCollectorSet |
TwoExpressionsCollectorSetList.findItem(int index)
Returns the object at the input index.
|
TwoExpressionsCollectorSet[] |
TwoExpressionsCollectorSetList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
TwoExpressionsCollectorSetList.append(TwoExpressionsCollectorSet object)
Appends an object to the list
License requirements: None. |
void |
TwoExpressionsCollectorSetList.append(TwoExpressionsCollectorSet[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
TwoExpressionsCollectorSetList.erase(TwoExpressionsCollectorSet obj)
Erases the object from the list, but does not delete the object.
|
void |
TwoExpressionsCollectorSetList.erase(TwoExpressionsCollectorSet obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
TwoExpressionsCollectorSetList.findIndex(TwoExpressionsCollectorSet obj)
Finds the index where the input object appears.
|
void |
TwoExpressionsCollectorSetList.insert(int location,
TwoExpressionsCollectorSet object)
Inserts an object at the specified location
License requirements: None. |
void |
TwoExpressionsCollectorSetList.setContents(TwoExpressionsCollectorSet[] objects)
Sets the contents of the entire list.
|
void |
TwoExpressionsCollectorSetList.swap(TwoExpressionsCollectorSet object1,
TwoExpressionsCollectorSet object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.