Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Method and Description |
---|---|
TransitionLawNodeBuilder |
MultiTransitionLawBuilder.createNode()
Creates a new law node
License requirements: solid_modeling ("SOLIDS MODELING") OR free_form_modeling ("FREE-FORM MODELING") OR studio_free_form ("STUDIO FREE FORM") . |
TransitionLawNodeBuilder |
TransitionLawNodeBuilderList.findItem(int index)
Returns the object at the input index.
|
TransitionLawNodeBuilder[] |
TransitionLawNodeBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
TransitionLawNodeBuilderList.append(TransitionLawNodeBuilder object)
Appends an object to the list
License requirements: None. |
void |
TransitionLawNodeBuilderList.append(TransitionLawNodeBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
TransitionLawNodeBuilderList.erase(TransitionLawNodeBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
TransitionLawNodeBuilderList.erase(TransitionLawNodeBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
TransitionLawNodeBuilderList.findIndex(TransitionLawNodeBuilder obj)
Finds the index where the input object appears.
|
void |
TransitionLawNodeBuilderList.insert(int location,
TransitionLawNodeBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
TransitionLawNodeBuilderList.setContents(TransitionLawNodeBuilder[] objects)
Sets the contents of the entire list.
|
void |
TransitionLawNodeBuilderList.swap(TransitionLawNodeBuilder object1,
TransitionLawNodeBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.