Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static SurfaceRangeBuilder.AnchorPositionType |
SurfaceRangeBuilder.AnchorPositionType.CENTER
Anchor at the center of the surface
|
static SurfaceRangeBuilder.AnchorPositionType |
SurfaceRangeBuilder.AnchorPositionType.VERTEX1
Anchor at the first corner of the surface
|
static SurfaceRangeBuilder.AnchorPositionType |
SurfaceRangeBuilder.AnchorPositionType.VERTEX2
Anchor at the second corner of the surface
|
static SurfaceRangeBuilder.AnchorPositionType |
SurfaceRangeBuilder.AnchorPositionType.VERTEX3
Anchor at the third corner of the surface
|
static SurfaceRangeBuilder.AnchorPositionType |
SurfaceRangeBuilder.AnchorPositionType.VERTEX4
Anchor at the fourth corner of the surface
|
Modifier and Type | Method and Description |
---|---|
SurfaceRangeBuilder.AnchorPositionType |
SurfaceRangeBuilder.anchorPosition()
Returns the anchor position
License requirements: None. |
static SurfaceRangeBuilder.AnchorPositionType |
SurfaceRangeBuilder.AnchorPositionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SurfaceRangeBuilder.AnchorPositionType |
SurfaceRangeBuilder.AnchorPositionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SurfaceRangeBuilder.AnchorPositionType[] |
SurfaceRangeBuilder.AnchorPositionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SurfaceRangeBuilder.setAnchorPosition(SurfaceRangeBuilder.AnchorPositionType anchorPosition)
Sets the anchor position
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.