Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static SupportPlaneData.LockPlaneStatus |
SupportPlaneData.LockPlaneStatus.AFTER_ALL_CONSTRAINT
Lock after all constraint
|
static SupportPlaneData.LockPlaneStatus |
SupportPlaneData.LockPlaneStatus.AFTER_FIRST_AND_SECOND_CONSTRAINT
Lock after first and second constraint
|
static SupportPlaneData.LockPlaneStatus |
SupportPlaneData.LockPlaneStatus.AFTER_FIRST_AND_THIRD_CONSTRAINT
Lock after first and third constraint
|
static SupportPlaneData.LockPlaneStatus |
SupportPlaneData.LockPlaneStatus.AFTER_FIRST_CONSTRAINT
Lock after first constraint
|
static SupportPlaneData.LockPlaneStatus |
SupportPlaneData.LockPlaneStatus.AFTER_SECOND_AND_THIRD_CONSTRAINT
Lock after second and third constraint
|
static SupportPlaneData.LockPlaneStatus |
SupportPlaneData.LockPlaneStatus.AFTER_SECOND_CONSTRAINT
Lock after second constraint
|
static SupportPlaneData.LockPlaneStatus |
SupportPlaneData.LockPlaneStatus.AFTER_THIRD_CONSTRAINT
Lock after third constraint
|
static SupportPlaneData.LockPlaneStatus |
SupportPlaneData.LockPlaneStatus.CENTER_POINT_DIRECTION
Lock support plane using center point and direction, this option should be used for Center Radius Arc only
|
static SupportPlaneData.LockPlaneStatus |
SupportPlaneData.LockPlaneStatus.LOCK_EXISTING_PLANE
Lock support plane using existing face or datum
|
static SupportPlaneData.LockPlaneStatus |
SupportPlaneData.LockPlaneStatus.NO
No Lock
|
Modifier and Type | Method and Description |
---|---|
SupportPlaneData.LockPlaneStatus |
SupportPlaneData.supportPlaneLockStatus()
Returns the support plane lock status
License requirements: None. |
static SupportPlaneData.LockPlaneStatus |
SupportPlaneData.LockPlaneStatus.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SupportPlaneData.LockPlaneStatus |
SupportPlaneData.LockPlaneStatus.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SupportPlaneData.LockPlaneStatus[] |
SupportPlaneData.LockPlaneStatus.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SupportPlaneData.setSupportPlaneLockStatus(SupportPlaneData.LockPlaneStatus lockPlaneStatus)
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.