Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static StepOptionBehavior.StepOptionType |
StepOptionBehavior.StepOptionType.EXTEND_NEIGHBORSAT_SMOOTH_EDGE
Extends faces neighboring a smooth edge of the motion face.
|
static StepOptionBehavior.StepOptionType |
StepOptionBehavior.StepOptionType.NONE
Does not add step faces.
|
Modifier and Type | Method and Description |
---|---|
StepOptionBehavior.StepOptionType |
StepOptionBehavior.stepOption()
Returns the step option
License requirements: None. |
static StepOptionBehavior.StepOptionType |
StepOptionBehavior.StepOptionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StepOptionBehavior.StepOptionType |
StepOptionBehavior.StepOptionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StepOptionBehavior.StepOptionType[] |
StepOptionBehavior.StepOptionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StepOptionBehavior.setStepOption(StepOptionBehavior.StepOptionType stepOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.