Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static SplineExtensionBuilder.ExtensionOption |
SplineExtensionBuilder.ExtensionOption.BY_POINT
Extend up to a point
|
static SplineExtensionBuilder.ExtensionOption |
SplineExtensionBuilder.ExtensionOption.BY_VALUE
Extend by value
|
static SplineExtensionBuilder.ExtensionOption |
SplineExtensionBuilder.ExtensionOption.NONE
No extension
|
Modifier and Type | Method and Description |
---|---|
SplineExtensionBuilder.ExtensionOption |
SplineExtensionBuilder.endExtensionOption()
Returns the extension options
License requirements: None. |
SplineExtensionBuilder.ExtensionOption |
SplineExtensionBuilder.startExtensionOption()
Returns the extension options
License requirements: None. |
static SplineExtensionBuilder.ExtensionOption |
SplineExtensionBuilder.ExtensionOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SplineExtensionBuilder.ExtensionOption |
SplineExtensionBuilder.ExtensionOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SplineExtensionBuilder.ExtensionOption[] |
SplineExtensionBuilder.ExtensionOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SplineExtensionBuilder.setEndExtensionOption(SplineExtensionBuilder.ExtensionOption extensionOption)
License requirements: features_modeling ("FEATURES MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
void |
SplineExtensionBuilder.setStartExtensionOption(SplineExtensionBuilder.ExtensionOption extensionOption)
License requirements: features_modeling ("FEATURES MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.