Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Method and Description |
---|---|
SpinePlaneBuilder |
Part.createEmptySpinePlaneBuilder()
Creates spine plane builder object
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
SpinePlaneBuilder |
SpinePlaneBuilderList.findItem(int index)
Returns the object at the input index.
|
SpinePlaneBuilder[] |
SpinePlaneBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
SpinePlaneBuilderList.append(SpinePlaneBuilder object)
Appends an object to the list
License requirements: None. |
void |
SpinePlaneBuilderList.append(SpinePlaneBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
SpinePlaneBuilderList.erase(SpinePlaneBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
SpinePlaneBuilderList.erase(SpinePlaneBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
SpinePlaneBuilderList.findIndex(SpinePlaneBuilder obj)
Finds the index where the input object appears.
|
void |
SpinePlaneBuilderList.insert(int location,
SpinePlaneBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
SpinePlaneBuilderList.setContents(SpinePlaneBuilder[] objects)
Sets the contents of the entire list.
|
void |
SpinePlaneBuilderList.swap(SpinePlaneBuilder object1,
SpinePlaneBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.