Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static SimpleDraft.SimpleDraftType |
SimpleDraft.SimpleDraftType.ASYMMETRIC
Draft on both sides of the profile using the not same angle
|
static SimpleDraft.SimpleDraftType |
SimpleDraft.SimpleDraftType.MATCHED_ENDS
Draft on both sides of the profile such that the end profiles match in areas
|
static SimpleDraft.SimpleDraftType |
SimpleDraft.SimpleDraftType.NO_DRAFT
No draft
|
static SimpleDraft.SimpleDraftType |
SimpleDraft.SimpleDraftType.SIMPLE_FROM_PROFILE
Draft using the profile as the reference
|
static SimpleDraft.SimpleDraftType |
SimpleDraft.SimpleDraftType.SIMPLE_FROM_START
Draft using the start limit as the reference
|
static SimpleDraft.SimpleDraftType |
SimpleDraft.SimpleDraftType.SYMMETRIC
Draft on both sides of the profile using the same angle
|
Modifier and Type | Method and Description |
---|---|
SimpleDraft.SimpleDraftType |
MultiDraft.draftOption()
Returns the draft type
License requirements: None. |
SimpleDraft.SimpleDraftType |
SimpleDraft.draftType()
Returns the simple draft type
License requirements: None. |
static SimpleDraft.SimpleDraftType |
SimpleDraft.SimpleDraftType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SimpleDraft.SimpleDraftType |
SimpleDraft.SimpleDraftType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SimpleDraft.SimpleDraftType[] |
SimpleDraft.SimpleDraftType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MultiDraft.setDraftOption(SimpleDraft.SimpleDraftType type)
License requirements: solid_modeling ("SOLIDS MODELING") . |
void |
SimpleDraft.setDraftType(SimpleDraft.SimpleDraftType type)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.