Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Method and Description |
---|---|
ReduceSurfaceRadiusFaceGroupBuilder |
CAMDataPrepManager.createReduceSurfaceRadiusFaceGroupBuilder()
Creates a
ReduceSurfaceRadiusFaceGroupBuilder
License requirements: None. |
ReduceSurfaceRadiusFaceGroupBuilder |
ReduceSurfaceRadiusFaceGroupBuilderList.findItem(int index)
Returns the object at the input index.
|
ReduceSurfaceRadiusFaceGroupBuilder[] |
ReduceSurfaceRadiusFaceGroupBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
ReduceSurfaceRadiusFaceGroupBuilderList.append(ReduceSurfaceRadiusFaceGroupBuilder object)
Appends an object to the list
License requirements: None. |
void |
ReduceSurfaceRadiusFaceGroupBuilderList.append(ReduceSurfaceRadiusFaceGroupBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
ReduceSurfaceRadiusFaceGroupBuilderList.erase(ReduceSurfaceRadiusFaceGroupBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
ReduceSurfaceRadiusFaceGroupBuilderList.erase(ReduceSurfaceRadiusFaceGroupBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
ReduceSurfaceRadiusFaceGroupBuilderList.findIndex(ReduceSurfaceRadiusFaceGroupBuilder obj)
Finds the index where the input object appears.
|
void |
ReduceSurfaceRadiusFaceGroupBuilderList.insert(int location,
ReduceSurfaceRadiusFaceGroupBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
ReduceSurfaceRadiusFaceGroupBuilderList.setContents(ReduceSurfaceRadiusFaceGroupBuilder[] objects)
Sets the contents of the entire list.
|
void |
ReduceSurfaceRadiusFaceGroupBuilderList.swap(ReduceSurfaceRadiusFaceGroupBuilder object1,
ReduceSurfaceRadiusFaceGroupBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.