Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Method and Description |
---|---|
PatternSpacingsListItem |
PatternSpacingsList.createPatternSpacingsListItem()
This is the default creator for
PatternSpacingsListItem . |
PatternSpacingsListItem |
PatternSpacingsListItemList.findItem(int index)
Returns the object at the input index.
|
PatternSpacingsListItem[] |
PatternSpacingsListItemList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
PatternSpacingsListItemList.append(PatternSpacingsListItem object)
Appends an object to the list
License requirements: None. |
void |
PatternSpacingsListItemList.append(PatternSpacingsListItem[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
PatternSpacingsListItemList.erase(PatternSpacingsListItem obj)
Erases the object from the list, but does not delete the object.
|
void |
PatternSpacingsListItemList.erase(PatternSpacingsListItem obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
PatternSpacingsListItemList.findIndex(PatternSpacingsListItem obj)
Finds the index where the input object appears.
|
void |
PatternSpacingsListItemList.insert(int location,
PatternSpacingsListItem object)
Inserts an object at the specified location
License requirements: None. |
void |
PatternSpacingsListItemList.setContents(PatternSpacingsListItem[] objects)
Sets the contents of the entire list.
|
void |
PatternSpacingsListItemList.swap(PatternSpacingsListItem object1,
PatternSpacingsListItem object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.