Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static PatternSpacing.SpacingType |
PatternSpacing.SpacingType.LIST
Specify offsets with a list.
|
static PatternSpacing.SpacingType |
PatternSpacing.SpacingType.OFFSET
Specify distance from the origin of one instance to the origin of the next instance.
|
static PatternSpacing.SpacingType |
PatternSpacing.SpacingType.PITCH
This is for pattern fill case.
|
static PatternSpacing.SpacingType |
PatternSpacing.SpacingType.PITCH_AND_SPAN
Specify distance between instances and distance for all instances, number of copies is calculated.
|
static PatternSpacing.SpacingType |
PatternSpacing.SpacingType.POLYGON_COUNT_PER_SIDE
This is for Polygon type.
|
static PatternSpacing.SpacingType |
PatternSpacing.SpacingType.POLYGON_PITCH_ALONG_SIDE
This is for Polygon type.
|
static PatternSpacing.SpacingType |
PatternSpacing.SpacingType.SPAN
Specify a distance for which all instances should occupy.
|
Modifier and Type | Method and Description |
---|---|
PatternSpacing.SpacingType |
PatternSpacing.spaceType()
Returns the type of spacing to be used by the pattern
License requirements: None. |
static PatternSpacing.SpacingType |
PatternSpacing.SpacingType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PatternSpacing.SpacingType |
PatternSpacing.SpacingType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PatternSpacing.SpacingType[] |
PatternSpacing.SpacingType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PatternSpacing.setSpaceType(PatternSpacing.SpacingType spaceType)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.