Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static PatternOrientation.ProjDirEnum |
PatternOrientation.ProjDirEnum.NORMAL_TO_FACE
project along face normal.
|
static PatternOrientation.ProjDirEnum |
PatternOrientation.ProjDirEnum.PATTERN_PLANE_NORMAL
use pattern plane normal as project direction.
|
static PatternOrientation.ProjDirEnum |
PatternOrientation.ProjDirEnum.RADIAL_DIR
project along radial direction.
|
static PatternOrientation.ProjDirEnum |
PatternOrientation.ProjDirEnum.USER_DEFINED_VECTOR
project along user defined vector.
|
Modifier and Type | Method and Description |
---|---|
PatternOrientation.ProjDirEnum |
PatternOrientation.followFaceProjDirOption()
Returns the followFaceProjDirOption, an enum for follow face project direction.
|
static PatternOrientation.ProjDirEnum |
PatternOrientation.ProjDirEnum.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PatternOrientation.ProjDirEnum |
PatternOrientation.ProjDirEnum.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PatternOrientation.ProjDirEnum[] |
PatternOrientation.ProjDirEnum.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PatternOrientation.setFollowFaceProjDirOption(PatternOrientation.ProjDirEnum followFaceProjDirOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") OR insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.