Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Method and Description |
---|---|
PatternIncrementItem |
PatternIncrementsList.createPatternIncrementItem()
This is the default creator for
PatternIncrementItem . |
PatternIncrementItem |
PatternIncrementsList.createPatternIncrementItem(Expression masterExpression)
This is the actual creator for
PatternIncrementItem . |
PatternIncrementItem |
PatternIncrementItemList.findItem(int index)
Returns the object at the input index.
|
PatternIncrementItem[] |
PatternIncrementItemList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
PatternIncrementItemList.append(PatternIncrementItem object)
Appends an object to the list
License requirements: None. |
void |
PatternIncrementItemList.append(PatternIncrementItem[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
PatternIncrementItemList.erase(PatternIncrementItem obj)
Erases the object from the list, but does not delete the object.
|
void |
PatternIncrementItemList.erase(PatternIncrementItem obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
PatternIncrementItemList.findIndex(PatternIncrementItem obj)
Finds the index where the input object appears.
|
void |
PatternIncrementItemList.insert(int location,
PatternIncrementItem object)
Inserts an object at the specified location
License requirements: None. |
void |
PatternIncrementItemList.setContents(PatternIncrementItem[] objects)
Sets the contents of the entire list.
|
void |
PatternIncrementItemList.swap(PatternIncrementItem object1,
PatternIncrementItem object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.