Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static PatternClockingBuilder.ClockingType |
PatternClockingBuilder.ClockingType.USER_DEFINED |
static PatternClockingBuilder.ClockingType |
PatternClockingBuilder.ClockingType.WITHIN_PATTERN_DEFINITION_CIRCULAR |
static PatternClockingBuilder.ClockingType |
PatternClockingBuilder.ClockingType.WITHIN_PATTERN_DEFINITION_LINEAR |
Modifier and Type | Method and Description |
---|---|
PatternClockingBuilder.ClockingType |
PatternClockingBuilder.clockType()
Returns the clocking enum to determine if linear or angular clocking
License requirements: None. |
static PatternClockingBuilder.ClockingType |
PatternClockingBuilder.ClockingType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PatternClockingBuilder.ClockingType |
PatternClockingBuilder.ClockingType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PatternClockingBuilder.ClockingType[] |
PatternClockingBuilder.ClockingType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PatternClockingBuilder.setClockType(PatternClockingBuilder.ClockingType clockType)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.