Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Method and Description |
---|---|
ParentEquivalencyMap |
ReplAsstBuilder.createEmptyMatch()
This is the default creator for a parent equivalency map.
|
ParentEquivalencyMap[] |
ReplAsstBuilder.createGeometricMaps()
Perform geometric matching.
|
ParentEquivalencyMap[] |
ReplAsstBuilder.createInferredMaps()
Infer more matches from matches already 'Accepted'.
|
ParentEquivalencyMap[] |
ReplAsstBuilder.createNameBasedMaps()
Perform automatic matching based on user-defined object names.
|
ParentEquivalencyMap |
ParentEquivalencyMapList.findItem(int index)
Returns the object at the input index.
|
ParentEquivalencyMap[] |
ParentEquivalencyMapList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
ParentEquivalencyMapList.append(ParentEquivalencyMap object)
Appends an object to the list
License requirements: None. |
void |
ParentEquivalencyMapList.append(ParentEquivalencyMap[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
ParentEquivalencyMapList.erase(ParentEquivalencyMap obj)
Erases the object from the list, but does not delete the object.
|
void |
ParentEquivalencyMapList.erase(ParentEquivalencyMap obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
ParentEquivalencyMapList.findIndex(ParentEquivalencyMap obj)
Finds the index where the input object appears.
|
void |
ParentEquivalencyMapList.insert(int location,
ParentEquivalencyMap object)
Inserts an object at the specified location
License requirements: None. |
void |
ParentEquivalencyMapList.setContents(ParentEquivalencyMap[] objects)
Sets the contents of the entire list.
|
void |
ParentEquivalencyMapList.swap(ParentEquivalencyMap object1,
ParentEquivalencyMap object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.