Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static OrientXpressBuilder.Plane |
OrientXpressBuilder.Plane.PASSIVE
Passive plane input mode
|
static OrientXpressBuilder.Plane |
OrientXpressBuilder.Plane.XY
Active plane is parallel to xy-plane
|
static OrientXpressBuilder.Plane |
OrientXpressBuilder.Plane.XZ
Active plane is parallel to xz-plane
|
static OrientXpressBuilder.Plane |
OrientXpressBuilder.Plane.YZ
Active plane is parallel to yz-plane
|
Modifier and Type | Method and Description |
---|---|
OrientXpressBuilder.Plane |
OrientXpressBuilder.planeOption()
Returns the orientXpress active plane option
License requirements: None. |
static OrientXpressBuilder.Plane |
OrientXpressBuilder.Plane.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OrientXpressBuilder.Plane |
OrientXpressBuilder.Plane.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OrientXpressBuilder.Plane[] |
OrientXpressBuilder.Plane.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
OrientXpressBuilder.setPlaneOption(OrientXpressBuilder.Plane orientXpressPlaneOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") OR insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.