Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static OrientXpressBuilder.Axis |
OrientXpressBuilder.Axis.PASSIVE
Passive axis input mode
|
static OrientXpressBuilder.Axis |
OrientXpressBuilder.Axis.X
Active axis in x-axis direction
|
static OrientXpressBuilder.Axis |
OrientXpressBuilder.Axis.Y
Active axis in y-axis direction
|
static OrientXpressBuilder.Axis |
OrientXpressBuilder.Axis.Z
Active axis in z-axis direction
|
Modifier and Type | Method and Description |
---|---|
OrientXpressBuilder.Axis |
OrientXpressBuilder.axisOption()
Returns the orientXpress active axis option
License requirements: None. |
static OrientXpressBuilder.Axis |
OrientXpressBuilder.Axis.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OrientXpressBuilder.Axis |
OrientXpressBuilder.Axis.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OrientXpressBuilder.Axis[] |
OrientXpressBuilder.Axis.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
OrientXpressBuilder.setAxisOption(OrientXpressBuilder.Axis orientXpressAxisOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") OR insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.