Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static MatchSurfaceBuilder.MatchConstaint |
MatchSurfaceBuilder.MatchConstaint.POSITION |
static MatchSurfaceBuilder.MatchConstaint |
MatchSurfaceBuilder.MatchConstaint.TANGENT |
Modifier and Type | Method and Description |
---|---|
MatchSurfaceBuilder.MatchConstaint |
MatchSurfaceBuilder.constraint()
Returns the continuity type for matching
License requirements: None. |
static MatchSurfaceBuilder.MatchConstaint |
MatchSurfaceBuilder.MatchConstaint.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MatchSurfaceBuilder.MatchConstaint |
MatchSurfaceBuilder.MatchConstaint.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MatchSurfaceBuilder.MatchConstaint[] |
MatchSurfaceBuilder.MatchConstaint.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MatchSurfaceBuilder.setConstraint(MatchSurfaceBuilder.MatchConstaint constraint)
License requirements: nx_freeform_2 ("advanced freeform modeling") OR die_engineering ("DIE ENGINEERING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.